7/20/2023 11:52 PM | |
Joined: 7/15/2021 Last visit: 6/12/2024 Posts: 4 Rating:
|
Hi and thanks in advance! I have a project in WinCC V7.5 SP2. Now I'm working on main menu. And have items related to alarm logging and tag logging. From my menu I can start AlarmControl with toolbar buttons pressed, i.e. alarm acknowledgement, therefore I conclude that controls can be accessed from main menu (using VBS). AlarmControls placed on pop-up picture window. At the moment I faced with problem accessing OnlineTrendControl from main menu (using VBS). I do can open specified picture window and make OnlineTrendControl visible, for example, but can't rich trend window or trend items. If I place a button on any pdl with script that shows needed trends - everything works well. Click on button >> another picture window with OnlineTrendControl opens, and I see all configured trends. If I add the script from button to VBS project module and start this module from main menu - I see empty trend window on specified picture window. How do I open picture window with configured trends from main menu? AttachmentMyScript_Trends.txt (152 Downloads) |
Last edited by: Mingshu28 at: 07/21/2023 00:12:35Last edited by: Mingshu28 at: 07/21/2023 00:13:40 |
|
Follow us on