7/5/2013 11:12 AM | |
Joined: 1/21/2013 Last visit: 6/2/2024 Posts: 4620 Rating: (705) |
Hi pobrien, In my opinion Wizard said DB no PB. Let us know if it works. Good luck |
7/5/2013 11:15 AM | |
Posts: 23 Rating: (0) |
Hi Ayman, An X-ref reveals that a read operation is executed on DB100.DBD50 at one location within the code. Thanks |
7/5/2013 12:01 PM | |
Joined: 1/21/2013 Last visit: 6/2/2024 Posts: 4620 Rating: (705) |
Hi Ayman, Ihope that our friend pobrien read it and see if he says his situation. |
7/5/2013 1:47 PM | |
Joined: 5/28/2008 Last visit: 6/3/2024 Posts: 4507 Rating: (837) |
Hello, As per my last post. If the old Panel (OP17) is damaged, then we have to read manuals to understand the area pointer structure. In any case,
Hope this helps. |
Ayman Elotaify |
|
1/2/2014 1:20 PM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating: (131) |
Hello Eng. Mohamed, have you solved your problem here? /tf/WW/en/Posts/101854#top It is lack of understanding of the structure of the area pointer! Screen entry no and Current field no are not the same!! Screen entry no is the no of the subscreen. In Protool is a BYTE, in WinCCflex is a INT. You are sure when you move INT to BYTE? Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de work faster withinnovative PLC-Tools |
1/27/2014 12:02 PM | |
Posts: 340 Rating: (6) |
new question is splittet to I want to change the OP177B to some other HMI. |
Follow us on