Industry Online Support
Technical Forum
7/10/2014 5:43 PM | |
Posts: 378 Rating: (73) |
Dear mjrv,
Yes you can back up by RS232/PPI cable. Create a new blank project wincc flexixible with your device type >> Project >> Transfer >> Backup , then follow the instructions. Note that you can only make backup if only the project was previously downloaded with back transfer option enabled. To restore: OP77, and OP277 are two different devices thus you need to reprogram/modify it to suit OP77 functions.
I am confused here, this OP277 is new? Without program? If no program, you can't see any user interface screens plus function keys are nothing without the program. Regards |
7/28/2014 9:52 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello mjrv, What WinccFlexible you have exactly? 2008 ---> SP? Update for WinCC flexible 2008 Service Pack 3 |
Last edited by: Ste39 at: 7/28/2014 9:58 AMUpdate SP3 |
|
Follow us on