10/29/2014 5:07 AM | |
Posts: 18 Rating: (0) |
helloSte39, i am trying with new cable, and then also it showing the same error, i am attaching the cable picture witch im using, in PROSAVE general tab after selecting OP77A ther are two BAUDRATE values are available, 57600 and 115200 witch one we have to select, is we need any changes according to this in our PC comport settings, please helpme for further. thanks & regards, chandu
|
10/29/2014 8:49 AM | |
Joined: 4/24/2006 Last visit: 9/25/2024 Posts: 8742 Rating: (1168)
|
Hello, Perhaps the following link might help: how can you transfer a WinCC flexible project serially to a panel? Only dip-switch for FREEPORT is relevant. Best regards, Wizard |
10/29/2014 9:53 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello chandu, Follow our Expert Wizard, (if you look in the previous posts you will find the same thing), and another thing, the LED on the converter as they are? |
10/29/2014 11:42 AM | |
Posts: 18 Rating: (0) |
helloWizardandSte39, thanq for ur reply, Wizardi dont have WINCC software, i am doing with PROSAVE, in this cable 6 dip switches are available, in that 4th switch is FREEPORT, i make that switch to '0' , in this when i power on the HMI the PPI indication leds is ON and while i enter start backup in prosave the TX led is blinking, but not the RX led, first i arrange HMI in "TRANSFER MODE" after that i entered the START BACKUP now the error is changed it is displaying like "A TIMEOUT ERROR HAS OCCURED WHILE SENDING THE FILES" i'm attaching the modem DIP SWITCHES and ERROR displaying SCREEN SCHOTS, please help me for further, thanks and regards, CHANDU.
AttachmentNew Folder (2).zip (148 Downloads) |
10/29/2014 3:05 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello chandu, I also have this PPI / Multimaster cable 6ES7 901-3CB30-0XA0 that unlike your has 8 dip switches "Made in Germany" (E-Stand 04) your "Made in China (E-Stand 05) but mine has the number 4 and 8 as a spare, so I think it is the same in the sense that my 5 is your 4 and my 7 is your 6, except that the first three are the baud rate, the other I have them all to 0, you tried it? I can not remember the last panel I've done, but tomorrow I have to go to a friend of mine who has an OP73 (which is similar), I will try with ProSave and we will list all the steps that I will to do the backup. Try your dip switches 5 and 6 to 0 "Zero" |
Last edited by: Ste39 at: 10/29/2014 4:36 PM |
|
10/30/2014 5:05 AM | |
Posts: 18 Rating: (0) |
helloSte39, thanq for reply, i tried with all the pins changing, thanks and regards, chandu
|
10/31/2014 7:05 AM | |
Posts: 18 Rating: (0) |
helloSte39,Wizard what i hv to do for further, is ther any changes required in PC settings ? please help me for further, thanks and regards
|
10/31/2014 8:56 AM | |
Joined: 4/24/2006 Last visit: 9/25/2024 Posts: 8742 Rating: (1168)
|
Hello, Try to lower the baudrate. and perhaps the following link might help: Why is the connection interrupted while transferring a project with ProTool to an OP? Best regards, Wizard |
11/1/2014 3:47 AM | |
Posts: 18 Rating: (0) |
thanq for replySte39andWizard, i tried the same process above you mentioned, im thinking PROSAVE V13.0.0.2is not supporting OP77A, kindly please provide me a older versions of PROSAVE. thanks and regards, chandu
|
Follow us on