3/17/2017 5:24 AM | |
Joined: 12/24/2014 Last visit: 5/17/2024 Posts: 14 Rating: (0) |
I also have the OPC problem updating the value of the tag. Connection with OPC server is good. I start Runtime. To check, I run the OPC-Scout-V10 and look at the value of the tag. The value of the tag has a start value and is no longer updated. If in the OPC scout press the button READ - then everything is fine, the tag is updated. As soon as we stop clicking the READ button - the tag value ceases to be updated. Installed the WinCC v7.2 - everything works well there, the tags are updated. I update to WinCC v7.3 - and there is such a problem. Why do not I update tags in WinCC v7.3? What is the problem? ------------------------------------------------------------------------------------------ |
Last edited by: Alexandr1984 at: 3/17/2017 5:26:17 AMLast edited by: Min_Moderator at: 3/17/2017 2:46:28 PMAdd attachment Last edited by: Min_Moderator at: 3/17/2017 3:01:19 PMNew subject after splitting |
|
Follow us on