9/25/2023 3:40 AM | |
Joined: 1/5/2023 Last visit: 3/29/2024 Posts: 1 Rating: (0) |
I am having this problem as well. I can open the project on some Engineering Station VMs that were created before we have record of what was done to set them up and install the specific configuration of PCS7. The engineering station I set up was a completely freshly installed image of Server2019. I was given the attached recommended PC7 installation configuration by a Siemens employee that is helping us out with integration. On this ES, and an other version of this VM setup but running Server2016, project archive retrieval yielded the error specified by OP. I also get the following error when trying to view the project:
I have added all users to user groups and given full read/write access to everyone for the entire C drive. I have tried retrieving the project to many places in the C drive as well as on secondary data-only (cold storage) drives. No idea why this keeps popping up. I can't recreate the error on the existing working (old) VMs that these new ones are supposed to replace. Ideas? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/25/2023 11:06:20Text formatting optimized. Last edited by: Jen_Moderator at: 09/25/2023 11:10:27New subject after splitting |
|
9/28/2023 9:01 AM | |
Joined: 1/11/2019 Last visit: 4/30/2024 Posts: 702 Rating: (140)
|
Hello, Please update the windows update and check. |
Follow us on