4/5/2013 1:09 PM | |
Joined: 8/31/2010 Last visit: 9/18/2024 Posts: 1521 Rating: (227) |
Hello suppaman87, Are your program blocks know how protected? As an excerpt from the system manual regarding "Opening projects from older versions of the TIA Portal" "● Projects from TIA Portal V11 Projects from version V11 are opened and remain unchanged. The range of functions is limited to the capabilities of TIA Portal V11. Projects therefore remain backwards compatible and can still be edited with the previous version of the TIA Portal. If you want to continue working on a project that you saved in TIA Portal V12 in TIA Portal V11, the most recent version of TIA Portal V11 must be installed. Service Pack 2 and all additional updates must be installed for TIA Portal V11. If you want to use all the functions of the current version in a project from TIA Portal V11, you need to upgrade the project. When you upgrade, the project is converted in the format of TIA Portal V12 and the full functionality of the TIA Portal V12 becomes available." There should not be a problem, but still if you are not able to get through I would suggest to Support Requestand then post the solution in this space |
Like it? Rate it! |
|
Follow us on