12/21/2017 4:17 AM | |
Posts: 33 Rating: (5) |
Hi Everyone, I'm working on OpenPCS7 accessing OSServer data OPCServerAE and OPCServerDA. For testing, I setup two virtual machines, one is for OpenPCS7 and the other is for PCS7 Engineering/Single Station. I follow all the procedures and requirements, where it must have the same workgroup, username/password, subnet. Connections are well established pinging on both sides and check if I can read/write all the shared folders, all are ok. So if you see the attached file, I use OPC Scout for OPC testing. So in the virtual machine (OpenPCS7 installed only), OPC Scout > Remote Server > OSServer, I can access both OPCServerAE and OPCServerDA. But when I try to access on Local Com Server or OPC Scout > Remote Server > Vmbox , it could not connect to the server so I can't access the data. Installed: Virtual Machine 1 - OS WinXP SP3 / OpenPCS7 / Simatic Net Virtual Machine 2 - OS WinXP SP3 / PCS Enigneering / OSSingle Station / Simatic Net I am just wondering, what did I missed in the setup. I also follow the steps on the link below.. https://support.industry.siemens.com/cs/ww/en/view/44444703 Advance thanks for the reply. |
Last edited by: Jen_Moderator at: 12/21/2017 2:24:58 PMInserted right link. |
|
Follow us on