1/10/2013 10:34 AM | |
Joined: 8/31/2010 Last visit: 9/18/2024 Posts: 1521 Rating: (227) |
Operating System Update for SIMATIC S7-1200 CPU Firmware V3 Update V3.0.2 The performance features supported by the firmware V3.0.2 of the S7-1200 CPU include:
Please note: The firmware of a V3 S7-1200 CPU can be updated via the integrated web server of the CPU or via FW-Update memory card. To perform the update via the web server of the S7-1200 CPU, the web server must be enabled. After a successful login the firmware can be updated via the menu item "Update Firmware". Overview of S7-1200 CPU order numbers for which this FW-Update is of relevance: Note: The software is subject to export restrictions, a download is only available to registered users. |
Like it? Rate it! |
|
5/9/2013 11:14 AM | |
Posts: 28 Rating: (0) |
Dear Pegaia, is it possible to update from firmware v2.2 to v3 Without Using Mmc Card (via Web Server)? |
7/22/2013 11:37 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Follow-up-question splitted to In my list of hardware does not have this option firmware (3.0.2) for CPU 6ES7 214-1AG31-0XB0 only 3.0 Best regards O_Moderator |
Follow us on