Industry Online Support
Technical Forum
11/18/2013 10:19 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
1. Create new project in your multiproject 2. Insert pc station 3. Open hardware and configure WinCC application for a server, WinCC application client for client etc... see manuals 4. Configure your terminal bus card...which is communicating with your AS... 5. Configure PC station (that is where the Station configurator comes into place.. (right click on your pc station-> PLC->Configure 6. After that, if configuration is possible-> PLC->Download.. Configuration is loaded to pc.. 7. Name your OS server (I assume you need a server), and enter symbolic name for it.. 8. set the download path Etc.. there are a few more steps like inserting connection in net pro between AS and OS... Please read the OS station configuration manual or Commisioning PC stations... |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on