7/17/2019 1:12 PM | |
Joined: 2/10/2010 Last visit: 11/24/2023 Posts: 77 Rating: (0) |
Hi I could not find any suitable conference, so I am posting it here. I was trying find any literature regarding parallel (enhanced) operation of SITOPs of different output capacity with same output voltage. But I can only find that two same SITOPs can be connected in parallel to double the available current, but can not find whether different rating SITOPs can be connected or not. Can anybody please provide some technical clarification regarding this matter? For example you can consider the following two SITOPs.
Thanks |
Follow us on