2/6/2019 6:35 AM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating:
|
Hello, check the windows device manager if the Adapter is correct installed here.
Christoph |
2/6/2019 11:17 AM | |
Joined: 7/9/2015 Last visit: 8/30/2024 Posts: 3943 Rating:
|
Hi, if PC Adapter ist installed without errors in Windows do the following Steps: - Check V5.6 Version-Update to SP1 it´s not installed yet. (Deactivate Virus Scanner if acitve) - If this does not help, check this FAQ: How do you generally parameterize the PG/PC interface and how do you ensure that the device driver can be selected and is visible?Regards, Towome |
|
|
2/7/2019 6:19 PM | |
Joined: 6/14/2015 Last visit: 9/3/2024 Posts: 242 Rating:
|
I have Simatic manager V5.6. I can connect with PLC. |
Follow us on