9/18/2015 9:35 AM | |
Posts: 567 Rating: (106) |
Hi it is normal. OB100 is the "start up" OB. If you stop the CPU und run it again the OB100 is called. If you open the block properties for example of an FB VlvL you see the field "To be insert in OB/Task". Have also a look in PCS 7 compendium part A and PCS 7 online help to get more Information about the OB 100. Link to PCS 7 compendium: https://support.industry.siemens.com/cs/de/en/view/107196780 |
9/18/2015 4:20 PM | |
Posts: 567 Rating: (106) |
Hi, how did you insert the blocks in the CFC? By drag and drop from library or are using CMTs?
|
Follow us on