11/26/2012 4:17 AM | |
Posts: 16 Rating: (0) |
Hello Experts I have went through mentioned manuals and configuration guides for PCS 7 CAS, and it always mentioned that CAS systems is equipped with client-servers structures. my questions is : PCS7 CAS can also work with a ' Multi-single OS stations' system?? my typical cofiguration is as attached. thanks for the help! AttachmentD:\Users\cn1jh160\Desktop\kaiquan\PCS7 Compendium\Multi oS single station PCS 7 V7.1 SP2].pdf (112 Downloads) |
11/26/2012 10:23 AM | |
Posts: 836 Rating: (100)
|
Hi, you have to use a seperate computer for a CAS. |
11/26/2012 2:26 PM | |
Joined: 10/26/2011 Last visit: 12/13/2024 Posts: 762 Rating: (192)
|
Hello, which PCS 7 version do you use? The CAS cannot handle Single Stations. If you use PCS 7 V8.0, then you can use the CAS replacement called Process Historian (PH). The PH supports Single Stations. Both the CAS and the PH must be installed on a separate PC. |
SIMATIC PCS 7 - Overview |
|
11/27/2012 10:24 AM | |
Posts: 140 Rating: (7) |
Hi, Why u r using 4 different Single OS stations, is the wincc project is getting different. Thanks, Surya. |
11/27/2012 1:14 PM | |
Joined: 10/26/2011 Last visit: 12/13/2024 Posts: 762 Rating: (192)
|
For a CAS you need a Server-Client architecture. In your case 1 OS server, 4 OS clients and 1 CAS. I am not sure, I think to have 4 OS clients and 1 OS serveris cheaper than 4 Single Stations. |
SIMATIC PCS 7 - Overview |
|
Follow us on