11/27/2014 12:26 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2167) |
Hello dzwilu, such a Mimimalkonfiguration is possible, here you can find more detailed information: http://support.automation.siemens.com/WW/view/en/24023824 Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
This contribution was helpful to1 thankful Users |
12/4/2014 2:22 PM | |
Joined: 10/26/2011 Last visit: 10/1/2024 Posts: 762 Rating: (191)
|
Hello dzwilu, did the link from dzwilu help you? |
SIMATIC PCS 7 - Overview |
|
12/18/2014 9:22 AM | |
Posts: 44 Rating: (2) |
Hi Guys, I have been trying to follow Chapter 5 of the manual linked above https://support.automation.siemens.com/WW/llisapi.dll/csfetch/24023824/24023824_PCS7_Mini_V80_en.pdf?func=cslib.csFetch&nodeid=65080933 I have a laptop set up as a temporary ES and two Siemens IPCs as the OS. The ES has a standard ethernet card and is connected to the CP1623s on the OS through a switch. I am only using TCP/IP communications, no ISO stuff... I can ping all three stations from all three stations / can ping by name All the stations appear as accessible nodes when I go to download to them. I can send configurations to each OS, which seem to be accepted However, I have two issues: 1. I am unable to download the WinCC project to either OS. Every time I try I get the following -“connection to the target module can not be established” 2. On page 63 of the above link it says to specify a path to the target computers. the IPCs I have bought have no shared folders on the network and (individually) no .MCP files on there. How do I get the project MCP files on to the OSs, in to a shared folder? I was under the impression that this could all be done remotely, from the ES, so that is what I am trying to do. Any help would be much appreciated. |
Last edited by: Min_Moderator at: 12/18/2014 2:50 PMChange link to permanent |
|
12/18/2014 9:57 AM | |
Posts: 567 Rating: (107) |
Hi DaltoneUK, you have to create a share folder by your own on your target system. On your ES you have to select the download path to this folder. You OS project will be saved as *.mpc file in this folder. On your ES the project is already a .*mcp. file. During the download the OS project will be copied from your ES to the OS-Station. Therefore a the windows mechanisms are used. Please have also a look to the PCS 7 compendium part A chapter OS download (your can see the necessary settings for OS download). http://support.automation.siemens.com/WW/view/en/107196780 |
12/18/2014 1:27 PM | |
Posts: 567 Rating: (107) |
Hi, check the settings of the terminal bus (advanced network settings of windows, Simatic shell,...).For OS download PCS 7 is using the terminal bus. If you don't have a terminal bus you should attend the recommendations of the following FAQ: http://support.automation.siemens.com/WW/view/en/43273606 |
This contribution was helpful to1 thankful Users |
12/19/2014 12:08 PM | |
Posts: 44 Rating: (2) |
Thanksa, that sorted it out! |
Follow us on