3/27/2010 12:19 AM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hi, I am Using the CP341 RS232 Modbus Slave With PCS7 V7.1 I try to Used the Block RCV_341 (FB121) which is Given in FAQ, But when I compile the CFC it is not parameterized "MODE", "SUBN1_ID", "SUBN2_ID", "RACK_NO" and "SLOT_NO", as per the FAQ it has to be Generated My CP 341MLFB No. 6ES7 341-1AH02-0AE0 So the above CP is supported by this Block (for generating the Module Driver), Because of this I am Not Able to Generate the Diagnostic Screen(Block Icon) on OS Side. But I am getting the Diagnostic For AS & OS object Which I configured in the Hardware Configuration. I am Using the 417-4H AS & PCS7 V7.1 Redundent Server & Client Configuration. & I have installed the all License Related to the Maintenance Station Runtime Package. any one face this Problem? |
Ammy |
|
Follow us on