7/19/2011 11:04 AM | |
Joined: 4/19/2008 Last visit: 6/25/2024 Posts: 1525 Rating: (159) |
Hi, Have a look on the following link SIMATIC PCS 7 V7.1 + SP3 Released for Delivery With what are SIMATIC PCS 7 V7.x, V 6.x, V5.x and V4.x compatible? |
Last edited by: Ammy at: 7/19/2011 11:05 AMAmmy |
|
7/19/2011 11:46 AM | |
Posts: 4 Rating: (0) |
Hello Ammy As I stated in my opening post, Iknowthe compability list. I am only interested in any experience on installing PCS7 on Windows Server 2008. |
7/20/2011 5:23 AM | |
Joined: 4/19/2008 Last visit: 6/25/2024 Posts: 1525 Rating: (159) |
Hi Jules, Requirements for installing and operating PCS 7 software V7.1 SP3 ● Windows XP Professional Service Pack 3 and Microsoft Internet Explorer V7. ● With Web Client and Web Diagnostics Client installations, Microsoft Internet Explorer V6 or V7 is permitted. ● Windows Server 2003 (Standard Edition) Service Pack 2 or Windows Server 2003 R2 Service Pack 2 (Standard Edition) and Microsoft Internet Explorer V7. ● Microsoft SQL Server 2005 Service Pack 3 is installed automatically. If the operating system is installed on the basis of Windows Server 2003 R2, we recommend that you do not enable the optional components of Windows Server 2003 R2. You will find the optional components of Windows Server 2003 R2 in the Windows Control Panel under Start > Settings > Control Panel > Add/Remove Programs > "Add/Remove Windows Components". You will find an overview and additional information on these Windows Server 2003 R2 options in Microsoft TechNet at If you are using an INTEL network card, install the driver stored under "Additional_Products\Drivers\NETWORK\Intel\Intel_LAN_v14.5.01_PROXP.exe" on the SIMATIC PCS 7 DVD. & you have already the list of upto PCS7 V7.1 SP2. insort it is not tested & not supported. |
Ammy |
|
Follow us on