4/30/2020 7:20 AM | |
Joined: 3/14/2008 Last visit: 8/10/2024 Posts: 2082 Rating: (931)
|
Hi, You can change the color in script: SSMGetButtonColor.fct in the following line:
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
5/1/2020 7:54 AM | |
Joined: 3/14/2008 Last visit: 8/10/2024 Posts: 2082 Rating: (931)
|
Hi, Hmm I have to check which script is responsible for that. The @PTN0 is created by the Picture Tree Manager, which is called during compile (if you check that option during compile). But the @logo should not be changed by compile. Only when you run OS project editor and checkmark the @logo.pdl (which means the pdl is taken from the library. You could overwrite the @logo in the SIEMENS directory, but with a new update, you must do this again.
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on