9/10/2020 12:33 PM | |
Joined: 9/27/2006 Last visit: 7/26/2024 Posts: 12270 Rating: (2676) |
Hello Amritpal; This page from the S7-1500R/H System manual shows that PID_Compact is available as a technology object on these CPUs, along with 2 other PID functions. https://support.industry.siemens.com/cs/ww/en/view/109754833/126307482251 Compare your program to the example presented and tell us if you see any difference to what you are doing. Hope this helps, Daniel Chartier |
9/11/2020 7:04 AM | |
Joined: 8/5/2014 Last visit: 7/26/2024 Posts: 160 Rating: (6) |
Hello dchartier, I have not done any programming in the project, i just create the new project and add the CPU model as mentioned, and tried to add the PID compact as mentioned in my last comment. Even unable to add PID compact from add new object in technology objects under the project tree. Please suggest.
|
Last edited by: Amritpal at: 09/11/2020 07:06:32Last edited by: Amritpal at: 09/11/2020 07:07:24Regards, |
|
9/11/2020 5:34 PM | |
Joined: 2/5/2013 Last visit: 7/25/2024 Posts: 320 Rating: (74) |
Check CPU firmware you need V2.8 Totally Integrated Automation Portal with STEP 7 Professional V16 or higher is required to configure this CPU firmware version. New features with firmware V2.8 for S7-1500R/H CPUs:
Br, AmolG |
Please rate it. |
|
This contribution was helpful to2 thankful Users |
9/14/2020 4:51 AM | |
Joined: 8/5/2014 Last visit: 7/26/2024 Posts: 160 Rating: (6) |
Hello AmolG, It means we can't use PID_compact from Tia V15.1 in CPU 1515R-2PN. We need to switch on Tia V16 for this?
|
Regards, |
|
9/14/2020 6:51 AM | |
Joined: 2/5/2013 Last visit: 7/25/2024 Posts: 320 Rating: (74) |
Hi, To use S7 1500 CPU with firmware V2.8 you need STEP 7 Professional V16 Br, |
Please rate it. |
|
9/14/2020 10:21 AM | |
Joined: 8/5/2014 Last visit: 7/26/2024 Posts: 160 Rating: (6) |
Thanks for the information.
|
Regards, |
|
Follow us on