Industry Online Support
Technical Forum
5/16/2012 8:52 AM | |
Joined: 6/26/2009 Last visit: 4/25/2024 Posts: 122 Rating: (23) |
Hi Ashutosh , I have this problem to , I already did some postings about it. You can find something here : PID not responding 1214 FW2.2 / V11 SP2 upd2 There is no need to write value 4 to the sRet_i_mode varaible. You can leave it on 3 and only set the "ManualEnable" bit to high if you want manual mode. I have the feeling that is more stabel this way , but not 100 % Also select the "enable lastmode after CPU restart " under basic settings. Please do some tests to and give us feedback. I see that V11 UPD3 and firmware 3 is comming soon , maybe it will be solved then. reagrds koenb. |
5/16/2012 9:41 AM | |
Posts: 18 Rating: (0) |
HiAshutosh , I have this problem to , I already did some postings about it. You can find something here : PID not responding 1214 FW2.2 / V11 SP2 upd2 There is no need to write value 4 to thesRet_i_mode varaible. You can leave it on 3 and only set the "ManualEnable" bit to high if you want manual mode. I have the feeling that is more stabel this way , but not 100 % Also select the "enable lastmode after CPU restart " under basic settings. Please do some tests to and give us feedback. I see that V11 UPD3 and firmware 3 is comming soon , maybe it will be solved then. reagrds koenb. Hi koenb, I allready writing only one value 3 tosRet_i_mode varaible and also allready selected"enable lastmode after CPU restart " under basic settings.which is allready instructed my Mr. Pegia. But still some times it goes in Inactive mode. I am using OB30 with 100ms and my cycle time is nearly 60ms. and problem is we can not wait for next update or new version coming from siemns. if you have update 3 for sp2 then please share the link with me hope it may help. Best Regards, Ashutosh. |
5/16/2012 9:58 AM | |
Joined: 6/26/2009 Last visit: 4/25/2024 Posts: 122 Rating: (23) |
here it is Update 3 for TIA Portal V11 SP2 please give us your feedback , I can't test now. |
1/4/2013 4:05 AM | |
Posts: 43 Rating: (0) |
Hi guys, My TIA Portal V11 sp2 has been updated with update 5. The problem still remain unchanged.. I am using ManualEnable to set PID mode Man/Auto but sret.i_mode change respectively. I mean sret.i_mode will change 4 when I set PID.MnaualEnable=TRUE. than i_mode remains unchanged (still 4) eventhough PID.MnaualEnable=FALSE. afterward when we write i_mode to become 3 it will go to 0 (PID is incative mode)... ... I've tried so many way, the only way is making i_mode not change to other mode when we are online and we do modify with trigger at i_mode. but it will gone as we offline it. I am still waiting Pegaia for his answer .... check pictures in attachment with modify with trigger Attachmentpictures.zip (202 Downloads) |
Last edited by: O_Moderator at: 1/7/2013 9:50 AM |
|
Follow us on