1/14/2015 3:21 PM | |
Posts: 211 Rating: (6) |
After upgrading TIAP V13 to TIAP V13 SP1 and then PLCSIM to PLCSIM V13 SP1, PLCSIM does not work. Reinstalling/modifying/uninstalling does not solve problem |
1/16/2015 2:04 PM | |
Posts: 211 Rating: (6) |
PUT/GET between two simulated S7-1200 worksfine. |
This contribution was helpful to1 thankful Users |
1/17/2015 9:44 AM | |
Posts: 211 Rating: (6) |
I simulated two s7-1200, exchanging data via Profinet. PLC1 is Controller, PLC2 is I device. Data exchange IS NOT simulated. |
5/26/2015 1:03 AM | |
Posts: 1 Rating: (0) |
Hi, when i saw in my registry files half of that i didnt got it. i tried to to write the same codes that you got.but doesnt solve the problrm |
Follow us on