5/10/2012 10:50 PM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
Hello Urban.matsson, How can you import tags from data blocks and from the symbol table into WinCC flexible version 2005 and higher? But I have never used this tool, Normally I Used the Second option Symbolic tag connection If you have integrated WinCC flexible in STEP 7, after importing you can run an automatic symbolic connection of the tags.
|
Ammy |
|
5/10/2012 11:02 PM | |
Posts: 16 Rating: (0) |
Hello Ammy, I can not get the second option working for PC, if I choose a panel it works ... I'm using WIndows 7 64 bits and STEP 7 5.5. Cheers Urban
|
5/11/2012 9:02 AM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
Hello Urban, If you intergate the WinCC Flexible Project in to the Step 7, when you Click on the Tag option let say I/O field then you can browse the all the DB which are available in the Step7. Just try it, right now I dont have WinCC Flexible installed on my Laptop other wise I will show you the Screen Shot for the same. also Which SIMATIC software can you install in 64-bit operating systems? for your ref. |
Ammy |
|
5/11/2012 9:26 AM | |
Posts: 16 Rating: (0) |
Thank you for your support! |
5/11/2012 9:34 AM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
there is a no need to Export the DB, Just intergrate your WinCC Flex project in Step7 How do you integrate a WinCC flexible project in STEP 7? then when you want to click on the Tag Dialog it will show you the DB which is available in the Step7 |
Ammy |
|
5/11/2012 10:06 AM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
Dear Urban, there is a always pain for the Tag Connection. Have a look on the How does tag multiplexing work? How does address multiplexing work? |
Ammy |
|
Follow us on