Industry Online Support
Technical Forum
12/23/2010 9:56 PM | |
Joined: 1/28/2009 Last visit: 6/1/2023 Posts: 6803 Rating:
|
Dear Just_Me I check all possiblity for missing code.This is my version. check the attachment for an illustrative analysis.When start signal activated,the preset value loads to accum and by each execution of block accum value counts down till zero which indicates waiting time finished.If the block is called in OB35 which is executed each 100ms (as an example), so for 2 second waiting time you need to load 20 in preset value.Note that the type of timer is on-delay in which by deactivating start signal , BR will be false and accum loads a high positive value. Hope this helps hdhosseini
AttachmentTIMER_ANALYSIS.zip (22 Downloads) |
Last edited by: hdhosseini at: 12/23/2010 10:15 PM |
|
Follow us on