4/13/2012 9:59 PM | |
Posts: 50 Rating:
|
Step # 7 of the WEB2PLC manual instructs the operator to in the HW configuration to doubleclick the CPU 317-2 PN/DP and select the WEB tab. Then it says to Activate the web server and it show a screen of what the options should be (see attached file). The only problem I have is the areas that I have highlighted in green can’t be accessed from my program, they are grayed out. In step 8 of the WEB2PLC program after you select ADD you start adding users. What can I do to gain access to the area highlighted in green? Attachmentweb2plc screen shot.pdf (431 Downloads) |
4/16/2012 8:54 AM | |
Joined: 10/10/2005 Last visit: 3/16/2023 Posts: 1909 Rating:
|
Hello, have you installed the following tools and moduls?
Further informations you will find in the following FAQ: http://support.automation.siemens.com/WW/view/de/51434100 With best regards |
Follow us on