8/15/2013 1:28 PM | |
Posts: 68 Rating: (7)
|
Creating new Applications, our colleagues are always giving thought to the same question: What kind of Application is better: A pdf , a video or maybe both? What would you prefer? A Video or a written pdf with some graphics? How many pages or what duration should those applications be at most? Please share your opinion! Find some example videos here: http://support.automation.siemens.com/WW/view/en/62102744 http://support.automation.siemens.com/WW/view/en/60978927 ...and some pdfs there: http://support.automation.siemens.com/WW/view/en/39863979 http://support.automation.siemens.com/WW/view/en/58862931 We're looking forward to getting your feedback! |
8/19/2013 9:36 AM | |
Joined: 10/3/2010 Last visit: 4/29/2024 Posts: 1552 Rating: (188) |
I would prefer both but with priority for pdf and video as a nice add-on (but as short as possible). |
B r g d s , |
|
This contribution was helpful to1 thankful Users |
8/21/2013 8:16 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hi FAQ-Expert My openion is the PDF ( With some Graphics / SCreenshots ) is a MUST !! We can work using the PDF alone althougha Video would be anicing on the cake Only Video would not be a practical option for me. Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
10/15/2013 3:45 PM | |
Joined: 1/28/2009 Last visit: 4/26/2024 Posts: 6838 Rating: (1359) |
Hello, This is my personal opinion that the visual presentation of technical issue will help newcomers to familiarize themselves very fast to the topic.But the most important point to be careful of the "Correctness" of information provided in webcasts as we frequently refer to them as starting point when it is asked in the forum.Complementary data in detail also can be available via PDF like before. But the combination as done HERE is also interesting. Best regards, Hamid Hosseini |
Follow us on