8/31/2017 11:24 PM | |
Posts: 8 Rating: (0) |
Hi!! I am doing a project in TIA Portal to control the motion of four stepper motors using technology objects. I have created a command table for each drive and I have two questions: Imagine if half way through of doing the instructions in the command table, there is an interruption that makes the motion stop. If the interruption is attended and whatever causing the interruption fixed, what will happen once we access the command table? Will it start from the beginning or from the point where it was interrupted? Thanks for the help!! ------------------- I splitted your questions. The other question is here: Position in Technology objects |
Last edited by: The Helping Hand at: 9/8/2017 2:20:00 PM |
|
Follow us on