3/21/2016 9:12 PM | |
Joined: 7/25/2011 Last visit: 9/11/2024 Posts: 20 Rating: (0) |
Hello. As always when I'm stuck, I try and always gets help in here I am trying to use the integrated technology objects PositionAxis in S7-1500, it looks quite good and useful for simple position tasks. In my project I have a G120 drive, Kübler profinet singel turn encoder and a S7-1500 PLC. I have set up everything according to some documents and tried a lot, and it almost work, I can start positioning and the drive goes to this position. But, the position is not correct, the encoder have 65536 pulses each round. In some way the position in Axis will not be the same as the encoder, in the axis there are decimals. When I go from position 0 to 1000, the encoder count to 65536 several times. As you can see in attached PDF the encoder position are correct in profidrive telegram, but not in the Axis control window. I dont know why, I have tried several settings without helping... I have created a link to project if someone want to see what I have done: https://www.dropbox.com/s/wbp5nqmctai7nqc/AbsolutePosisjonering_V1.zap13?dl=0 Have someone seen anything like this or know why this is happening, please help me Thanks in advanced, Andreas Frebrich
AttachmentEncoder.pdf (544 Downloads) |
Follow us on