10/24/2014 12:48 PM | |
Joined: 10/24/2014 Last visit: 6/29/2024 Posts: 4 Rating: (0) |
Hello dear all, I am using a CU305-DP with a CPU-313C 2-DP and Telegram 111 to control a rotary axis where 1 load turn is 3600 LU. I have already made all the traversing block programming but when I start the axis, it stop beyond the progamation. It takes around 16 turns more than I have programed. The TrvBlock 0 works fine. The problem happens when I use the TrvBlocks 1 to 3, because I need speeds, acc and dec diferents in each part of the move without stop the axis. Someone could help me please?
AttachmentPictures.zip (101 Downloads) |
11/4/2014 3:12 PM | |
Joined: 10/24/2014 Last visit: 6/29/2024 Posts: 4 Rating: (0) |
I alreadychecked, I put speed and acc/deceleration in 100%, but the result was the same. |
Follow us on