7/4/2015 7:42 AM | |
Joined: 5/7/2015 Last visit: 9/20/2023 Posts: 56 Rating: (1) |
Hi friends, Basically, going by all that is said above.. I've ended up dragging the elements of the PLC's data-block( Not the DB itself) into the HMI's tag table. This is perhaps inelegant but a practical way.. as the HMI tags can't have a dot in them so" structure.element" gets converted to "structure_element" Next, I wish to attach a pop-up screen to my faceplate. In my project there are about 60 on-off valves. I have made the face-plates to which I assign the interface tags for each valve. Now I haven't figured out a way to assign these to a single pop-up screen. I am reading up on SmartTags which seem to convert strings to tags. Is it possible for pop-up screens to use smart-tags associated with the interfaces of faceplates?
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/6/2015 11:40:46 AMNew subject after splitting |
|
This contribution was helpful to1 thankful Users |
7/29/2015 8:58 AM | |
Joined: 4/26/2006 Last visit: 7/11/2023 Posts: 1 Rating: (2) |
Dear Raj First sorry for my English! I’m also a beginner in TIA13 WinCC and I have exact the same problem like you. Here I present my solution where I made in the last two weeks but WITHOUT ANY GUARANTE for success!!! First you see my Valve-Button. When I press this Button the Valve Button will open the dynamic Valve-Popup (see picture Valve_Popup). I draw this Valve_Popup under “Pop-Up-Pictures”. In the picture “Valve_Button” you can see what “commands” the Valve-Button have. I send the tagname to a VB-Script an in the VB-Script the tagname will put together to a real tag (SmartTag). On the picture “Valve_Popup” you can see Buttons. When I press one of this Buttons an action will start (see picture “Valve_Popup_Button_Command”). The Button-Commands activate the VB-script. For the Valve states on the Valve_Popup I used “multiplexing” (see picture “Variable_Multiplexing”). I hope you can follow my steps. Best regards Patrick
AttachmentValvePopup.zip (1300 Downloads) |
This contribution was helpful to3 thankful Users |
6/30/2017 10:29 AM | |
Joined: 6/19/2017 Last visit: 4/26/2024 Posts: 7957 Rating: (162) |
New question published by Zhanelya is split to a separate thread with the subject Can pop-up screens use smart-tags associated with the interfaces of faceplates?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on