Industry Online Support
Technical Forum
7/27/2011 10:22 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, 1. Look at http://support.automation.siemens.com/WW/view/en/42480411 http://support.automation.siemens.com/WW/view/en/23369901 2. There is need to assign the connection in WinCC FLex. 3. Yes. Best regards, Hristo Mihalev |
7/27/2011 10:26 AM | |
Joined: 4/29/2010 Last visit: 3/19/2024 Posts: 1557 Rating: (161)
|
Hello, to 1.) This is limited by the maximum number of connection resources from the cpu/ from the CP. This FAQ explains this a bit (just to understand what connection resources means): What is the maximum number of OPs that a CPU S7-300 can communicate with? to 2.) What you you mean there detailed? Sure it is possible and should do so. best regards |
7/27/2011 11:35 AM | |
Posts: 3 Rating: (0) |
Thanks very much! |
Follow us on