12/10/2008 10:23 AM | ||||
Joined: 5/28/2008 Last visit: 12/8/2015 Posts: 901 Rating: (136) |
Hello faming, Application Disconnects the connection to the PLC in use and establishes a new connection to the given PLC. The "ChangeConnection" function is used to interconnect an HMI device with a PLC at a different address.
The follows address types are supported:
The follows PLC types are supported:
Syntax ChangeConnection (Connection, Address, Slot, Rack) Useable in script: Yes (ChangeConnection) Parameters Connection Name of the PLC to which the connection is to be established. The name is determined during configuration in the connection editor. Address MPI/PROFIBUS or IP address of the PLC to which the connection is to be established. Here you also get informations: http://support.automation.siemens.com/WW/view/de/22584322 http://support.automation.siemens.com/WW/view/de/23842653 I hope it is enough to configure the connection... regards manfred Ho Ho Ho |
|||
Last edited by: *Manfred* at: 12/10/2008 10:37 AM |
||||
12/12/2008 1:47 AM | |
Joined: 6/8/2007 Last visit: 4/12/2024 Posts: 41 Rating: (1) |
Thanks for your answer, really helpful.. |
Follow us on