Industry Online Support
Technical Forum
10/1/2013 8:29 AM | |
Posts: 12 Rating: (0) |
Hello, I am working with Tia Portal V12 WinCC Basic. I have a project with KTP600 PN, CPU Vipa. My problem comes when I try to simulate the project. The panel opens and I can read "Checking project ID...". After 5 seconds more or less I read the following: "Cannot get Project ID" and the window Run Time closes "shutting down". When does it normally happen? What have I wrong done? Thank you so much, Javier AttachmentGanzseitiges Foto2.pdf (303 Downloads) |
10/1/2013 9:56 AM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (41) |
Hello, is the message a system message or it is a created message by yourself/ someone else? Because I did not see a message viewer. Do you have a connection to the plc? Did it works in the past? Regards, healthcheck |
Grundkurs/Systemkurs WinCC V7: |
|
Follow us on