11/23/2011 2:19 PM | |
Joined: 9/19/2011 Last visit: 11/11/2024 Posts: 140 Rating: (33) |
What version of firmware do you have in the 231-5QD30 module? If you do not have V01.00.05 then see this link to upgrade. https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&nodeid0=41886031&nav0=tree&lang=en&siteid=csius&aktprim=0&extranet=standard&viewreg=WW&objid=41885258&treeLang=en This should fix the problem that you are seeing. |
11/23/2011 6:06 PM | |
Posts: 1 Rating: (0) |
make sure that you ground the module and connect the M of the 24V Supply to the same ground instruction sheet for module should provide additional details |
11/24/2011 1:09 PM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating: (153) |
Have you measured TCs too see if they are floating type or they are grounded? |
Follow us on