Industry Online Support
Technical Forum
7/13/2021 12:56 PM | |
Joined: 7/10/2017 Last visit: 8/4/2022 Posts: 2 Rating: (0) |
Good day everyone! I need to access the parameters of the SEW UHX65 controller. For this I decided to use the "SEW_MOVI-C_SingleParameterAccess" library downloaded from the SEW official site. But nothing works for me. As I see, the problem is in the access of the WRREC \ RDREC functions to the Profinet bus. I tried setting the "Allow reconfiguration of device via the user program" option, it didn't help. My equipment: 1) CPU 1518F-4 PN / DP 2) SEW UHX65 I would be very grateful for any help or ideas!
AttachmentTest_ProfinetIO_SEW_SPA.zip (317 Downloads) |
7/13/2021 5:56 PM | |
Joined: 7/10/2017 Last visit: 8/4/2022 Posts: 2 Rating: (0) |
Also if i change library version from 1.1 to 1.0 i receive message illustrated on picture bellow. This make me confused. |
9/23/2024 1:11 PM | |
Joined: 10/18/2013 Last visit: 9/23/2024 Posts: 2 Rating: (0) |
Hello, I'm having same problem more or less with a UXH65 and FB200 to write/read. It doesn't work. Have you solved it? |
Follow us on