11/20/2007 11:21 AM | |
Posts: 7 Rating:
|
Hi, I am using Ethernet module (6GK7-343-1EX30-0XE0) with S7-300 315 CPUs. I would like to exchange data between 2 PLCs. Simple program is attached herewith. There are problems with data exchange. Every time I get error 8183H (Configuration missing). I have defined IP address in hardware configuration, Is there any other settings I have to do in hardware configuration?? I am using FC5 (AG_SEND) in one PLC and FC6(AG_RECV) in another PLC, and ID is mentioned IP adress of Ethernet module for other PLC. Regards, Guru AttachmentEthernet.zip (497 Downloads) |
Last edited by: gururaj at: 20.11.2007 11:24Last edited by: gururaj at: 20.11.2007 11:23 |
|
11/20/2007 1:37 PM | |
Joined: 4/24/2006 Last visit: 2/7/2025 Posts: 8839 Rating:
|
Hello Guru, Have you seen these faq's: http://support.automation.siemens.com/WW/view/en/19062476 http://support.automation.siemens.com/WW/view/en/8707570 http://support.automation.siemens.com/WW/view/en/26708188 Here is an example: http://support.automation.siemens.com/WW/view/en/17853532 Did you configure a Connection in Netpro? Best regards, Wizard |
11/24/2007 8:34 AM | |
Posts: 7 Rating:
|
Thanks, It worked with "GET", "PUT" FB's regards, |
Follow us on