Industry Online Support
Technical Forum
7/10/2014 9:26 AM | |
Posts: 3 Rating: (0) |
Hi all, I have a strange problem with faceplate script. In the project at the _MAIN screen there's 2 buttons, one of them is in faceplated which executes a script on button click and the other button is a normal button which executes similar script outside the faceplate. When I start this project on simulator, neither of the script are executed on button click, however if I delete faceplated button the second script works fine. However if I redo all this in a new project everything is working fine, even the faceplate is working. Please don't tell me to use InvertBit function, this is just an example of a problem I have, I need to execute a larger script, which is also not working. Thank you in advance. Project was to large to attach so I uploaded it on dropbox, here's the link: [snip ...] AttachmentD:\tmp\upload\TEST_SCRIPT.zip (139 Downloads) |
Last edited by: CS Moderator at: 7/10/2014 12:41 PMProject attached |
|
Follow us on