9/24/2009 2:53 PM | |
Joined: 7/13/2009 Last visit: 10/7/2024 Posts: 137 Rating: (5) |
Dear All, We are having 20 numbers of Simatic Field PGs M2 with Step5 V7.23 installed. S5 is working fine in all the PGs in Adminstrator Login mode(Windows). But S5 is giving some error as mentioned in the screen shots in User Login Mode(Windows) only in 4 no of PGs and after acknowledging the error Step5 is opening but not going to online with PLC. There is no problem with other 16 no of PGs with any user login(Windows). Im attaching screen shots of the error and registry file of one of the PGs with problem. Plz help us to solve the problem. Attachment_PG details.zip (267 Downloads) |
Thanks and Regards |
|
10/13/2009 9:24 AM | |
Joined: 7/13/2009 Last visit: 10/7/2024 Posts: 137 Rating: (5) |
Dear All, I got the following reply for the above said problem from siemens plz try this http://support.automation.siemens.com/WW/view/en/18700465 Regards, Manjunath |
Thanks and Regards |
|
Follow us on