7/24/2013 10:01 AM | |
Posts: 61 Rating: (0) |
Hello everyone, I have 2 motors, there job is to blow when some process end. They are working separately in circuit mode M1,M2,M1,M2.... The main program is not important, what am I trying to do is when M1 is in ERROR (temperature, current, etc protection activates) program give command to M2 to start and inverse, when M2 is in ERROR to start M1. I just write a test program to see how it will work, but M2 is working, M1 won't start. Can please someone tell me what am I doing wrong or if someone have some better solution. Best regards, G.P. AttachmentFC99.pdf (58 Downloads) |
7/24/2013 10:28 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi Have you tried in Online if the contacts goes inon state? |
Last edited by: Ste39 at: 7/24/2013 10:32 AM |
|
7/24/2013 10:45 AM | |
Posts: 61 Rating: (0) |
Contact ERROR_M2 is now going in state that it saved by (#) ERROR_M2. I don't understand why? AttachmentMOTOR STATE.pdf (56 Downloads) |
7/24/2013 11:16 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi Have you tried to reverse the networks? The network 2 over the network 1? |
7/24/2013 2:02 PM | |
Posts: 61 Rating: (0) |
Here is a final FC, I don't need timer in this program. I have one existing input from timer to reset motor.
AttachmentFC99final.pdf (54 Downloads) |
Follow us on