2/9/2010 3:07 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
can someone answer this? see above I have the same problem--> with SelA02IN block (switch between two analog values) |
Last edited by: O_Moderator at: 2/10/2010 12:55 PMLast edited by: O_Moderator at: 2/10/2010 12:53 PMnew subject after splitting from /tf/WW/en/Posts/20663#top If I could help you, you can use the RATE button. Thank you. |
|
2/9/2010 3:32 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
stupid, I'm looking at a CFC printout from version 4.0 A level is measured with DIG_MON and the output is connected to the Analog switch. If the level is high,the switch is enabled so IN2 is selected instead of IN1. And your done..... just a BOOL as input to switch... |
Last edited by: O_Moderator at: 2/10/2010 12:55 PMIf I could help you, you can use the RATE button. Thank you. |
|
2/11/2010 7:42 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
hello, The problem was not solved... I meant that in version 4.0, you just could connect with a BOOLtype toanalog switch, but in 7.1 you have to have aSTRUCT type. But how to use a struct is unknown to me... so if somebody knows a answer.. Thx |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on