Industry Online Support
Technical Forum
9/29/2010 1:12 PM | |
Posts: 2 Rating: (0) |
I'm having similar problem as well with my reserve acting linear actuators. The feedback from the Iy unit to DCS is correct but the position feedback shown on the Sipart PS2 is reverse (i.e. When valve is fully closed, feedback shown in DCS is 0% but feedback shown on Sipart PS2 is 100% and vice versa). I have tried to change the parameter 7(Setpoint direction) and parameter 38( Direction of manipulated variable for display) but the results is the same. The problem only occurs with my reverse acting linear actuators. The direct acting actuators are fine. Appreciate if someone who have faced similar problem and resolved it could advice what can be done ;) Power cycling andreinitializationdoesn'tsolve the problem as well.
Splitted from Sipart PS2 Strange Beahveour. |
Last edited by: O_Moderator at: 9/30/2010 9:45 AMnew subject after splitting Last edited by: sridaran at: 9/29/2010 1:20 PM |
|
Follow us on