10/7/2019 3:05 PM | |
Joined: 4/20/2017 Last visit: 9/17/2024 Posts: 81 Rating: (6) |
Hi guys I am trying same thing for encoder calibration of S120s drives.. And I have serious problems with that.. This is my configuration: CPU 315-2 PN/DP, SINAMICS CU320 with Infeed and 3x S120.. Like you can see on screenshot..PLC project is in TIA Portal 13 SP2.. I am controlling servos by SINA_POS FB.. It works well. Now I wan to make encoder calibration from PLC... I tried to use SINA_PARA_S FB for that, but it was not possible, because it is using WRREC 1.1 and I have HMI Lite 6.2 used in this project which use WRREC 1.0.. And if I tired to set globally WRREC 1.0 for whole project, then it is not possible to compile, because HMI Lite FBs are protected.. So I was searching for solution couple of days downloading manuals, listing forums, etc..And I found that, how to use SFC 58 / 59... So I prepare everything for test.. I tried to read some parameter from last S120 in HW config, but with no success... I stuck on WR_REC ret_val:16#8093 value.. And now I do not know what to do / what is wrong.. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/07/2019 16:44:36New subject after splitting |
|
10/7/2019 3:05 PM | |
Joined: 4/20/2017 Last visit: 9/17/2024 Posts: 81 Rating: (6) |
|
10/7/2019 3:07 PM | |
Joined: 4/20/2017 Last visit: 9/17/2024 Posts: 81 Rating: (6) |
|
10/7/2019 5:09 PM | |
Joined: 8/21/2014 Last visit: 9/19/2024 Posts: 1024 Rating: (14) |
Closed because question was posted multiple times. Please use: trying to use SFC 58 to calibrate encoder on S120 |
My Forum is the place to personalize your profile, |
|
Follow us on