9/1/2016 4:03 PM | |
Posts: 17 Rating:
|
Hi again! 2. CPU lke Client So, let's start. 1.Situation: SF is blinking with error in Module Information Buffer about no license. Question: If i use DEMO from here DEMO MODBUS TCP does my system must work if fields of my DB3 "License DB" - empty? Check pic.1 in attachments. 2. Situation: I have DB with array of 30 word's and i want to sent this data to OPC. Question: I use only 1 DB so, acording to manual i need too use Holding Regiters from 40001 - 40031 on OPC? According to manual from previous link, i need to config first 2 parametrs in instance DB. But, look at the code under, in DB102 (instance DB fo FB) or in DB1 "C.Data" wich i use for relations on my OB1 for CALL FB102? DB102 and DB1 - the same! "C_Data" - DB1
So, do i need to configurate this DB's on stay it alone? 4. Situation: Server or Client? Question: According to manual i can use TCP wizard or config by myself. Client or Server is depend form next settings: - active_est (active/passiv connection) -local_tsap_id_len -rem_tsap_id_len -server_client |
9/1/2016 4:06 PM | |
Posts: 17 Rating:
|
It's my project in Client configuration. Also, do i need to do omthing on Network and hardware configuration? Add some devices and etc.. ? AttachmentTest_3_1.zip (145 Downloads) |
Last edited by: Sapher_Jalt at: 9/1/2016 4:12:17 PM |
|
9/5/2016 8:20 AM | |
Joined: 1/27/2015 Last visit: 7/22/2024 Posts: 53 Rating:
|
Hi Sapher_Jalt,
Greez Bachgeist |
This contribution was helpful to
1 thankful Users |
Follow us on