3/21/2022 8:50 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (216) |
Hi NoorKhan, the question is not so easy to answer. Which topology do you want? Which devices do you want to use? The best way to start with the topic topology is with the application example PROFINET in Process Automation with SIMATIC PCS 7. There you can find lot of example configuration and detailed configuration guideline for the ET200SP HA. Also you can find a good description for the configuration S1, S2, R1, MRP, CiR and SoE. With regards |
This contribution was helpful to1 thankful Users |
Follow us on