1/7/2018 8:36 PM | |
Joined: 9/27/2006 Last visit: 5/26/2024 Posts: 12257 Rating: (2668) |
Hello narove; Which model of Lantec burner controls are you working with? There seems to be a few models on the market. For example, this document describes the Etamatic burner controls Profibus configuration, but states that the file to be requested has a DMD extension; the screenshots of the configuration seem to show that the DMD file includes the required gsd files http://lamtec.su/download/Etamatic/BUS/BA-Profibus-DLT6100-EN.pdf There is contact information for Lamtec in the creenshot below, or you could use their website to start a support request: https://www.lamtec.de/en/topmenu/kontakt.html Hope this helps, |
Last edited by: dchartier at: 1/7/2018 8:37:53 PM |
|
1/7/2018 11:05 PM | |
Joined: 9/27/2006 Last visit: 5/26/2024 Posts: 12257 Rating: (2668) |
Hello narove; You should contact Lamtec to request the CD or the gsd (DMD?) file for your unit. You can register on the Lamtec.de site to download the BT300 manual in English or German. You will be required to create a user login to obtain the manual, it is a very quick operation. https://www.lamtec.de/en/service-and-support/downloads.html In the manual you will find Profibus comm. tables for input bytes (from the BT300 to the master) and output.(from the master to the BT300) bytes. As you can see from the screenshot below, the BT300 offers 60 input bytes (0-59) of data that will be read by the master. There is another table showing 14 output bytes, commands from the master to the BT300. From the screenshot that you received in the previous post, you see that the ETAMATIC Profibus chips supports bus speeds up to 1,5MB; check out similar indications in the BT300 gsd file. Simply choose which one you will use for the network and set that vlue in the master's Profibus parameters. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 1/8/2018 11:38:54 AM |
|
Follow us on