5/10/2017 2:09 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating:
|
Hello, |
With best regards... |
|
5/10/2017 2:19 PM | |
Joined: 9/27/2006 Last visit: 6/13/2024 Posts: 12260 Rating:
|
Hello exester; Here are 2 FAQs that show how to setup: 1- an Unspecified partner on S7-connections (this is necessary for PUT and GET functions) How you configure a connection in the TIA Portal?(pay attention to point 7). 2- a program for PUT and GET functions between 2 S7-1200 CPUs. This sample is more complex than you need, since it involves a sequncer that calls 3 instances of GET and 3 instances of PUT functions one after the other. For your requirements, concentrate on the first PUT and the first GET calls. Hope this helps, Daniel Chartier |
This contribution was helpful to
1 thankful Users |
5/10/2017 10:02 PM | |
Posts: 2826 Rating:
|
You are being lazy. Working through the "noise" is required to understand the functionality. Attached is a Step7 V13 SP1 example without the "noise". Sadly the code is untested - these cannot be simulated and needs actual hardware. It is a ZAP13 archived project that has been ZIPed. Use the menu option in TIA Portal: Project > Retrive.. to extract the ZAP13 file to a project. If you need explanations, it means you need to work through the "noise". The PLC manual is also equally qualified to explain what you need to know. Regards
AttachmentGetPutSample.zip (1496 Downloads) |
5/11/2017 4:12 PM | |
Joined: 3/23/2012 Last visit: 2/7/2024 Posts: 23 Rating:
|
Hello #dP, Lazy is not a nice word, I spend hours of reading and testing before i go to the forum in the hope somebody has had the same problem and solved it easy. See the attached pictures, it went already wrong with selecting the area, and if it is possible to select it should work. Who can advise me it the right way but without telling that somebody is lazy or is stupid? AttachmentPUT-GET.pdf (2062 Downloads) |
Follow us on