3/13/2024 8:20 PM | |
Joined: 1/21/2013 Last visit: 4/26/2024 Posts: 2714 Rating: (440)
|
Hi, First of all, yes, it is possible to set dynamic units within a faceplate at will. I have seen this in several projects. Looking at your script example, I think the problem is that you are trying to write the unit to the process value, and then use the process value - which should be the unit, not the process value - to change the output format. I have not tried this myself, but I am pretty sure it cannot work. I suggest that you try the following approach.
If this still does not work, please provide more information about the values inside the script using the debugger. Kind regards |
This contribution was helpful to1 thankful Users |
Follow us on