3/25/2015 2:03 PM | |
Joined: 5/28/2008 Last visit: 9/11/2024 Posts: 1343 Rating: (141)
|
You need to setup in the hardware configuration of the input you like to use for PWM. With the CTRL_PWM block you only control the signal. Please have a look in the manual or here https://support.industry.siemens.com/cs/de/de/view/63200733/en |
This contribution was helpful to1 thankful Users |
3/26/2015 7:11 AM | |
Posts: 5225 Rating: (1192) |
Hi. The description is contradictory.[LINK] "0 to 400Hz" is stating a PTO where the frequency is varied. PWM is where the ON-OFF cycle ratio (duty cycle) can be changed. Thereafter.. look at [LINK] w |
Follow us on