4/8/2013 8:20 AM | |
Posts: 37 Rating: (3) |
Sorry i misunderstud you. But if the sensor maximum measure is 40m (20mA). Then if you use the same sensor for a watter level of only 20m then it shoul transmit 12mA. It's simple math. You have a range of 16mA for 40m...how much for 20m? 16/2=8mA, 8mA+4mA (offset)=12mA. Same for 10m (read 8mA) and for 15m (shoul read 10mA). look athttps://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW&objid=10805397&treeLang=en |
4/11/2013 5:21 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715)
|
Hello, I believe the mA is not that important, you need to know how it's represented in the PLC as Int. Here is how to convert the signal into meters(or whatever you need) How can you scale analog values with S7-200 in conjunction with CPU224XP and expansion modules EM 231, EM 232 and EM 235? Regards, Marcjan |
Problem solved? |
|
Follow us on