4/26/2012 11:58 AM | |
Posts: 21 Rating: (0) |
Thank you again Darius I will try with SSL4692 as soon as possible. Bye @LAD |
4/26/2012 1:00 PM | |
Joined: 9/28/2005 Last visit: 8/27/2024 Posts: 2957 Rating: (242)
|
Put feedback here once you make test. Its interesting for me too |
Best regards, |
|
4/26/2012 3:12 PM | |
Joined: 10/7/2005 Last visit: 9/22/2024 Posts: 3021 Rating: (1054)
|
Hello @LAD the CP342-5 is a bit of a "special" external DP master interface and even though I've never tried using SFC51 on it to read the status of itsDP Slaves, I wouldn't be suprised if it doesn't work (please try though by any means and let us know the result). In caseyou can't make it to work, I suggestyou grab FC3 "DP_DIAG" from the "SIMATIC_NET_CP/CP 300" library and use it instead and below is also a link with more on it (it's pretty simple to use though and should give you all the info you are after): CP 342-5 -- How do you recognize the failure of a DP slave operating on CP342-5? I hope this helps |
Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on