6/26/2009 2:09 PM | |
Posts: 510 Rating: (117) |
Report System Error will allow you to capture the information on an exception basis. http://support.automation.siemens.com/WW/view/en/22727527 On the high end Maintenance Station can provide information with the automatic generation of a maintenance overview in WinCC from the STEP 7 hardware configuration. Here is a link http://support.automation.siemens.com/WW/view/en/34291015 |
6/26/2009 2:17 PM | |
Posts: 691 Rating: (36) |
Report System Errorwill create alarms in WinCC But I want to Show the Status of the PLC with the modules connected with it in the Runtime Screen |
6/26/2009 4:36 PM | ||||||
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hi Ninja, here link of previus tread Hardware diagnostics in WinCC runtime
Hope can help Regards |
|||||
This contribution was helpful to2 thankful Users |
6/27/2009 7:41 AM | |
Posts: 691 Rating: (36) |
Thank U CBo for this tool But I can't get the status of the modules which are there in the CPU Rack ( Rack 0) like SM and CP Modules |
6/27/2009 3:36 PM | |
Posts: 261 Rating: (42) |
Hi CBo, Thanks. The link is a miracle. Thanks again. With warm regards ddg |
Last edited by: ddg at: 6/27/2009 3:39 PM |
|
6/28/2009 1:57 PM | |
Joined: 10/7/2005 Last visit: 5/18/2024 Posts: 3005 Rating: (1048) |
Hello Ninja Robot this may not be what your are after since it will give access to the HWconfig but if you already have Step7 installed on you WinCC PC you could simply add a button to the WinCC system thatcalls it (you''ll find S7HWCNFX.EXE in the /BIN folder of your S7 installation). It's a cheap and "nasty" way of achievingquick and easy access to HWconfig related online diganostics and will only work on PC's that have Step 7 and access to the PLC's, nonetheless it may be what you are after (from memorythere are also switches that will makeit openright away in online view, if only I could remember where I had that info ..). |
Cheers |
|
7/1/2009 1:54 PM | |
Joined: 2/6/2009 Last visit: 5/7/2024 Posts: 938 Rating: (118) |
Hi Ninja, Please find the below link for Previos Threads about the Hardware Diagnostics in WinCC. /tf/WW/en/Posts/30561#top Please find the below link for the ET 200M Diagnostics . /tf/WW/en/Posts/30955#top |
Last edited by: saravana kumar@VAES-Bangalore at: 7/1/2009 1:56 PM_______________________________________________________________ |
|
7/1/2009 2:58 PM | |
Posts: 691 Rating: (36) |
Is there any method described in the link about reading the module information other than CPU in Rack 0 I can't see |
Follow us on